Sample Deployment Architectures
The following examples show different types of deployment architectures to use with the MQTT Client. Configuration Hub and Proficy Authentication are installed only once in each architecture.
Example 1
The following example shows Configuration Hub, Proficy Authentication, and the MQTT Client
installed with SCADA in one computer.

Example 2
The following example shows Configuration Hub, Proficy Authentication, and the MQTT Client
installed in one computer, and SCADA on different computer.

Example 3
The following example shows Configuration Hub and Proficy Authentication in one computer
and another computer with SCADA and the MQTT Client.

Example 4
The following deployment architecture illustrates Configuration Hub, Proficy
Authentication, SCADA, and the MQTT Client are installed on separate computers.