You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
In the Operations Hub installation folder, open the windows.env file in a text editor.
Note: We recommend that you back up the original windows.env file.
As needed, provide values for the parameters, and save the file.
Open Command Prompt, and run the following command: <Operations Hub installation folder>\OpHub-Windows-Installer>ophub_bundle <switch>, where <switch> is one of the following values:
-q, -quiet, -s, -silent: Use one of these values to initiate the automated installation.
-passive: Use this value if you want progress bar to appear during the installation.
-norestart: Use this value if you do not want services to be restarted during the installation.
-promptrestart: Use this value if you want a message to appear, asking whether services must be restarted.