Triggering/Non-triggering SQL Queries
This topic describes the SQL triggering and non-triggering functionality.
- Operations Hub Classic version, accessible under Query definition and Page designer.
- Specifically designed for input plug-ins (excluding widgets).
When creating SQL queries in Operations Hub, you have the option to specify whether
the SQL query should be triggered or not when a change occurs in its input value.
You can also specify if the value is mandatory or optional to trigger a query. By
default, the options are set to Triggering
and
Optional
for all SQL queries. This is also the default behavior
of Operations Hub page designer PAGE DATA tab >
Query option > Auto submit on input
change.

Non-triggering
If the input parameter is set to Non Triggering
, then at runtime any
change to the input does not trigger the query.
Triggering
If the input parameter is set to Triggering
, then at runtime any
change to the input will trigger the query provided all the mandatory fields are
set.
Optional
If the input parameter is set to Optional
, then the input need not
have any value for the query to trigger.
Mandatory
If the input parameter is set to Mandatory
, then the input should
contain a value for the query to trigger.