Configure automatic logout

Configure automatic logout if you want Workflow to automatically log out the user after a specified period of inactivity. When you configure automatic logout on a global basis, the specified timeout applies to all computers that are configured to use the global settings.

Procedure

  1. In the navigator, click Proficy System > Proficy System > Computers.
  2. From the Computers list, select the computer that you want to configure.
    Tip:
    If you are configuring settings for all computers in your system or a subset of those computers, you can skip this step. However, you can still configure global default settings if you select an individual computer.
  3. In the Displays panel, select the editor you want to use.
    To configure autologout on...Select
    an individual computerComputer Editor
    all computers or a subset of computers in your systemDefault Computer Editor
  4. Click the Login/Logout Configuration tab.
  5. In the Auto Logout section, select the Enable Auto logout check box.
  6. In the Timeout in section, enter the number of minutes and/or seconds representing the amount of time that Workflow can remain open without activity before automatically logging the user out of the system.
    Note:
    User activity is defined as moving or clicking the mouse, or pressing keyboard keys.
  7. Click Save.
  8. Restart the Workflow client for the autologout settings to take effect.