APM System Monitoring
Deploy APM System Monitoring for the First Time
About This Task
The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.
These tasks may be completed by multiple people in your organization. GE Digital recommends, however, that the tasks be completed in the order in which they are listed.
| Step | Task | Notes |
|---|---|---|
| 1 | On the machine that will serve as the APM System Monitoring Server, download and install the latest version of MongoDB Community Edition. | This step is required. The latest version of MongoDB Community Edition, as well as instructions about how to install it, can be found on the official MongoDB, Inc. website. Note that instructions for configuring a Windows Service for MongoDB Community Edition are provided in the next step. |
| 2 | Configure a Windows Service for MongoDB Community Edition. | This step is required. |
| 3 | On the machine that will serve as the APM System Monitoring controller, install APM System Monitoring. | This step is required. |
| 4 | On each machine that will serve as an APM System Monitoring agent, install APM System Monitoring. | This step is required. |
| 5 | On the machine that will serve as the APM System Monitoring admin, install APM System Monitoring. | This step is required. |
| 6 | Complete additional configuration steps related to APM System Monitoring. | This step is required. |
| 7 | As needed, modify APM System Monitoring settings via the Performance Monitoring feature. | This step is optional. |
Upgrade or Update APM System Monitoring to V4.6.0.0.0
About This Task
The following tables outline the steps that you must complete to upgrade this module to V4.6.0.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Procedure
Configure a Windows Service for MongoDB
Before You Begin
- On the machine that will serve as the APM System Monitoring Server, download and install the latest version of MongoDB Community Edition.
Procedure
What To Do Next
- Return to the APM System Monitoring first-time deployment workflow.
Install APM System Monitoring
Before You Begin
- Complete all previous steps in the APM System Monitoring first-time deployment workflow.
Procedure
What To Do Next
- Return to the APM System Monitoring first-time deployment or upgrade workflow.
Configure APM System Monitoring
Procedure
What To Do Next
- Return to the APM System Monitoring first-time deployment or upgrade workflow.