Reliability Centered Maintenance

Deploy RCM for the First Time

Before You Begin

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.

These tasks may be completed by multiple people in your organization. GE Digital recommends, however, that the tasks be completed in the order in which they are listed.

Results

Step

Task

Notes

1

Assign Security Users to one or more of the RCM Security Groups and Roles.

This step is required.

2

Review the RCM data model to determine which relationship definitions you will need to modify to include your custom equipment and location families. Via Configuration Manager, modify the relationship definitions as needed.

This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families.

Upgrade or Update RCM to V4.6.0.0.0

Before You Begin

The following tables outline the steps that you must complete to upgrade this module to V4.6.0.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Procedure

  • Upgrade from any version V4.5.0.0.0 through V4.5.0.0.9

    This module will be updated to V4.6.0.0.0 automatically when you update the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V4.4.0.0.0 through V4.4.0.0.13

    This module will be updated to V4.6.0.0.0 automatically when you update the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V4.3.0.0.0 through V4.3.1.0.11

    This module will be updated to V4.6.0.0.0 automatically when you update the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V4.2.0.0 through V4.2.0.9.5
    StepTaskNotes
    1Prior to upgrading your database, review any RCM Analysis records that are linked to virtual assets. If you want any of those analyses to remain an analysis, link the associated virtual assets to the Asset Hierarchy prior to upgrading.

    In addition, for any analyses that are linked to both real and virtual assets, link all the virtual assets in the analysis to the Asset Hierarchy prior to upgrading.

    This step is required only if your database has virtual assets linked to an RCM analysis, and you do not want the analysis to be converted to an analysis template on upgrading.
  • Upgrade from any version V4.1.0.0 through V4.1.7.4.0

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V4.0.0.0 through V4.0.1.0

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V3.6.1.0.0 through V3.6.1.7.5

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V3.6.0.0.0 through V3.6.0.12.9

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V3.5.1 through V3.5.1.12.3

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V3.5.0 SP1 LP through V3.5.0.1.10.1

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V3.5.0 through V3.5.0.0.7.1

    This module will be upgraded to V4.6.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.

  • Upgrade from any version V3.4.5 through V3.4.5.0.1.4
    StepTaskNotes
    1Assign Security Users to the MI RCM Viewer Security Group.This step is required.
    2Add values to the Recommended Resource System Code Table.This step is required. This System Code Table is used to populate the Recommended Resource field in RCM FMEA Recommendation records.