Reliability Analytics
Deploy Reliability Analytics for the First Time
Before You Begin
The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.
These tasks may be completed by multiple people in your organization. GE Digital recommends, however, that the tasks be completed in the order in which they are listed.
Results
Step | Task | Notes |
---|---|---|
1 | Review the following data models to determine which relationship definitions you will need to modify to include your custom equipment and location families:Via Configuration Manager, modify the relationship definitions as needed. |
This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families. |
2 | Assign Security Users to one or more Reliability Analytics Security Groups and Roles. | This step is required. |
3 | Ensure that the Meridium Simulation Service is installed and running. | If the basic GE Digital APM system architecture is already installed, the Meridium Simulation Service is automatically installed and run. |
Upgrade or Update Reliability Analytics to V4.6.0.0.0
Before You Begin
The following tables outline the steps that you must complete to upgrade this module to V4.6.0.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.