AlarmItemClick
AlarmItemClick triggers a procedure or script that can provide a list of information when a user clicks an alarm in the Alarm Viewer control.

Field | Description | |||
---|---|---|---|---|
Event | ActiveX Event provides the AlarmItemClick expression. | |||
ActiveX Event | AlarmItemClick is included in the drop-down list. | |||
Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||
Procedure | Create or use an existing procedure. | |||
Script | Create or use an existing script. | |||
Parameter | Can be used if the event invokes a script directly or through a procedure. The default code begins as follows. Private cimOleObj As AMVOCXLib.IAmvOcx Sub OnAlarmItemClick(AlarmInfo As AMVOCXLib.AmvOcxAlarmItemInfo, ClickSource As Long) Where parameters are: | |||
AlarmInfo | Object that accesses several properties as follows. | |||
Property | Description | |||
String AlarmIdentifier() | Alarm ID | |||
String ResourceIdentifier() | Resource ID | |||
String ReferenceIdentifier() | Reference ID | |||
String Project() | Project name | |||
Date GenerationTime() | Date/time the alarm was generated | |||
Long AlarmState() | Alarm state | |||
Long AckState() | Acknowledge state | |||
String AlarmScreen() | (For point alarms only) Screen that is associated with the point on the Point Properties dialog box View tab. | |||
Long Severity() | Alarm severity | |||
String AlarmMessage() | Alarm message | |||
Long Duration() | Alarm duration | |||
String TranslatedAlarmMessage() | Alarm message translated into the language specified for screen on which the alarm is selected. Important: The language and translated string must be in the CIMPLICITY Language Mapper to display correctly. | |||
ClickSource | Source that was used to click on an alarm in the Alarm Viewer list. The source is identified as follows. | |||
Source | Identified by | |||
Left-mouse button | 0 | |||
Right-mouse button | 1 | |||
Enter key | 2 | |||
Note: The AlarmItemClick event will not be fired for the right-mouse button if the Context (Popup) menu is enabled for the Alarm Viewer control.
The Popup menu can disabled by clearing either of the following check boxes.
|
||||
Checkbox | Location | |||
Right click menu | Privileges tab in the Role Properties dialog box. | |||
Allow runtime popup menu | Display tab in the CIMPLICITY AMV Control Properties dialog box. |