NewAlarm
NewAlarm triggers a procedure or script when a new alarm is received or when an existing alarm has a state change.

Field | Description | |
---|---|---|
Event | ActiveX Event provides the NewAlarm expression. | |
ActiveX Event | NewAlarm is included in the drop-down list. | |
Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |
Procedure | Create or use an existing procedure. | |
Script | Create or use an existing script. | |
Parameter | Can be used if the event invokes a script directly or through a procedure. The default code begins as follows. Private cimOleObj As AMVOCXLib.IAmvOcx Sub OnNewAlarm(NewAlarms As Boolean, AlarmCount As Long, AlarmDate As String) Where parameters are: | |
NewAlarms | True if a new alarm was received. | |
AlarmCount | Number of alarms being displayed. | |
AlarmDate | Time stamp of the alarm update or new alarm. |