Relative setpoint adds the offset value to the current value of the point. The result is downloaded to the point.
Configure the action as follows.
1
Action type
2
Point ID
3
Offset
4
Confirmed
Select Relative setpoint.
Point on which a setpoint is performed.
Offset values must be integers or real numbers.
Point must be a Read/Write point.
Opens the Select a Point browser.
Opens a Points Popup menu.
Number added or subtracted from the point's value when a user
Clicks the Up/Down arrows in the default box.
Presses the Up/Down arrow keys.
(Optional) Runtime confirmation.
Checked
Requires confirmation.
A message box will display before the action occurs requesting confirmation to proceed.
Clear
Does not require confirmation.
Default
Clear