Alert Template

Configure the Default Alert Template

About This Task

This topic describes how to configure the settings for the default alert template that you can use with analytic templates and deployments.

Procedure

  1. In the Applications menu, navigate to RELIABILITY > Analytics > Configuration.
  2. Expand Alert Template.
  3. Enter values as described in the following table.
    FieldDefinition
    Alert Template ConsumableIndicates whether the alerts associated with the alert template will be consumable or non-consumable. For more information, refer to Create, Configure, or Delete an Alert Template.
    Alert Template SeverityThe severity that you want to associate with the applicable triggered alerts. Enter a value between 1 and 5.
    Alert Template SourceThe analytic source that you want to associate with applicable alerts.
    Note: When creating a template, you can select manual from the source list. When you do so, you can create alerts that do not come from a typical source.
    Alert Template TripDesignates the trip association for alerts requiring immediate action.
    Alert Template TypeThe alert type for the analytic to associate with applicable alerts.
  4. Select Save.
    The default alert template is configured.