Template Type | Identifies the default Analytics Template data frame type used while uploading the template. You can enter one of the following values:- Shared Time Stamp
- Per Port Time Stamp
- HierarchicalType
- DescriptiveType
|
Output Tag Format | Indicates whether the output tags are used as DynamicMapping or AssetTagMapping. |
Custom Attributes | Indicates whether you want to enable adding custom attributes under filters. |
Disable Asset Level Cache | Indicates whether GEDA Asset query calls are cached to load asset filter data. If you want to use cache, set this field to false. |
Scheduled Run Logs Limit | Identifies the asset-level deployment logs entries that contain input and output json files. You can enter a value up to 20. We recommend that you enter 3. |
Lines of Analytic Logs | Identifies Analytics run log line limit. The default value is 1000 and the permissible value can range between 0 to 10000. |
Maximum Asset Selection Count | Identifies the maximum number of assets that appear in the ASSET FILTER field while selecting an asset in the Deployments section. We recommend that you enter a maximum value of 1000. |
Trigger Deployment Per Template | Identifies the number of deployments that are triggered from ingested Time Series data for each template. |
Trigger Deployment Count | Identifies the total number of deployments used in a given tenant. |
Trigger Deployment Auto Delete | Indicates whether the trigger for deployment must be automatically deleted. |
Analytic Runtime Resources Dynamically Editable | Identifies whether analytics resources can be updated. |
Minimum Schedule Time | Identifies the least scheduling frequency in minutes for a deployment. We recommend that you maintain a high value for Analytics frequency so that there is a sufficient duration between last execution and next execution times of scheduled Analytics. |
IO Upload | Indicates whether you can upload CSV files for IO Mapping fields on inputs, constants, and output. |
Success Log Enable | Indicates whether info logs must be generated for each selected asset for deployment. You can set this value to enable deployment issue diagnosis. To avoid extra logging and runtime performance issues, we recommend that you set this field to false. |