Creating and Managing Custom Folders

Folder Management allows you to organize plugins with custom folders in the NAVIGATION panel.

Procedure

  1. Click the overflow icon next to the search field.
  2. Select Create New Folder and enter a name.

    The folder appears under plugins.
  3. Use the overflow menu on folders to:
    • Create child folders
    • Rename folders
    • Delete folders
  4. Move plugins between folders using the Move to folder option.
    Note:
    • If you want to delete a child folder but have any plugin(s) under it, clicking the overflow icon of the child folder and selecting the Delete option will display a warning message: Deleting this folder will also delete its child folders and move the plugins under them to the root. Do you want to continue? with the options Yes or No. If you select Yes, the plugins under the child folder will be moved to the root level.
    • You do not have the option to delete the plugins directly. You must unregister the product plugins to remove them from the NAVIGATION panel.
    Important:
    Refer to Troubleshooting Folder Management Errors to resolve folder management related issues.