Overview of CIMPLICITY in Configuration Hub

Configuration Hub allows you to configure your Proficy products all together in one place, and access and configure them from anywhere. You can manage multiple Proficy products, including CIMPLICITY, from within Configuration Hub. For instance, Proficy Authentication, Operations Hub, and Historian.

After registering CIMPLICITY plug-in with Configuration Hub, you can log in to Configuration Hub, either using the desktop shortcut on the Configuration Hub machine desktop, or from the CIMPLICITY Workbench. For more information on registering the plug-in, see About Registering the CIMPLICITY Plug-in.

The CIMPLICITY plug-in appears in the Navigation pane, along with its associated projects on the left-side panel as shown in the following figure.
Note:
To access the plug-in, you must have the SCADA.COMPUTER@[NodeName].$CONFIGSECGRP scope published to Proficy Authentication. By default, all the needed scopes are added to the ch_admin user.
Marker Description
1 CIMPLICITY Node/ computer registered with Configuration Hub and Proficy Authentication.
2 Project associated to the CIMPLICITY node.
3 Devices associated to the project.
Note:
Connections is displayed only if a Project is configured with devices. You can click Connections to browse devices and create points.