Select and Browse Devices
About this task
Procedure
-
In the machine that has Configuration Hub installed, in the desktop, double-click
.
Alternatively, in the CIMPLICITY node machine, you can open Configuration Hub from the Workbench.The Proficy Authentication login page appears.The Configuration Hub page appears, listing all the CIMPLICITY nodes and their associated plug-ins in the NAVIGATION pane.
Marker Description 1 CIMPLICITY Node/ computer registered with Configuration Hub and Proficy Authentication. 2 Project associated to the CIMPLICITY node. 3 Connections is displayed only if a Project is configured with devices. You can click Connections to browse all the available devices and create points. -
From the left pane, expand the required project and select
Connections.
The devices tab appears, listing all the associated devices.
Marker Description 1 List of all the OPC UA devices associated to the project. 2 Details of the selected device. Note:This is read-only.In case of a redundancy project, you can see the details like node name, status, and path of the configured primary and secondary servers.
3 Column chooser. You can select what all information of a device you want to view in the grid. Available options:- Device ID
- Network Address
- Description
- Port Type ID
-
Select a device, and then select the ellipsis (...) to the right of your
entry.
A popup menu appears.
-
From the popup menu, select Browse.
A new tab appears, listing the device and all its associated objects.Note:If you are already browsing a device, you will be prompted with a popup stating that you are already browsing a device and whether you want to replace it. If you select Yes, the existing device tab is replaced with the selected device.
You can now create SCADA points from the objects displayed for the selected device.