Start and Stop a CIMPLICITY Project

About this task

You can start a project and stop a running project from Configuration Hub. In case of a Redundant server configured project, you will have additional options to start or stop projects at the primary or secondary level.
Note:
If you have set the CIM_SSL_STRICTPOLICY parameter to Y (recommended), it is important that the primary server trusts the secondary server's SSL certificate, and vice versa.

To start a project, perform the following:

Procedure

  1. In the machine that has Configuration Hub installed, in the desktop, double-click .
    Alternatively, in the CIMPLICITY node machine, you can open Configuration Hub from the Workbench.

    The Proficy Authentication login page appears.

  2. In the NAVIGATION pane, select and expand the required node.
    All the associate plug-in and its projects are listed.

  3. Select a project, and then select the ellipsis (...) to the right of your entry in the Actions column.
    Alternatively, you can right-click on the required project and select the actions as needed.
    A popup menu appears.
  4. Select an action as needed.
    The below table explains the available options:
    Option Description
    Start Select this to start a stopped project.
    Stop Select this to stop a running project.
    Start Primary and Secondary Select this to start a stopped project in both primary and secondary servers.
    Start Primary Select this to start a stopped project in primary server only.
    Start Secondary Select this to start a stopped project in secondary server only.
    Stop Primary and Secondary Select this to stop a running project in both primary and secondary servers.
    Stop Primary Select this to stop a running project in primary server only.
    Stop Secondary Select this to stop a running project in secondary server only.
    If you select Stop, a confirmation popup appears. Select Yes to stop the project.