Classifications Inherited Attributes

Access Inherited Attributes for a Classification

You can access inherited attributes for a classification. When a child-classification is created, all the custom attributes in the root-classification are copied to the inherited attributes.

About This Task

Inherited attributes appear only for asset or tag classifications. You can enter a new value or modify an existing value for an inherited attribute. You cannot add or delete an inherited attribute from the classification view. It can only be deleted from the root-classification.
Note: Root-classification does not have inherited attributes.

Procedure

  1. In the Applications menu, navigate to HEALTH > Assets > Classifications.
  2. Find and select a classification in the Classifications results table.
  3. Scroll down to Inherited Attributes to access the following information:
    FieldDescription
    Attribute NameThe name of the attribute appears.
    ValuesThe value or values of the attribute appears.

Add or Modify Inherited Attribute Values for a Classification

You can add or modify an inherited attribute value for a selected root-classification or a child-classification.

Procedure

  1. In the Applications menu, navigate to HEALTH > Assets > Classifications.
  2. In the Classification results table, select the classification to which you want to add or modify inherited attribute values.
  3. In the Inherited Attributes section, hover over and select an attribute value.
  4. In the Value box, enter a new value, and then press ENTER or select outside the box.
    The new value is added.
    Alternatively, you can hover over a reserved attribute value, select , and then enter a value in the Attribute Value Definition box.
    Note: You cannot change the datatype of the attribute.
  5. Select Save.
    The entered value is saved and appears in the Value column for the selected reserved attribute.