Classifications Reserved Attributes

Add or Modify Reserved Attribute Values for a Classification

You can enter or modify reserved attribute values for an asset or tag classification.

About This Task

Reserved attributes are system defined attributes. These attributes only appear for asset or tag classifications. You can enter a new value or modify an existing value for a reserved attribute. You can add new values or modify existing values for a reserved attribute that contains . Reserved attributes have predefined formatting which cannot be modified. You cannot add or delete a reserved attribute, or modify the name of the reserved attribute.

Essentials Asset has identified a list of reserved attributes for Asset and Tag classifications. To ensure that you do not add custom attributes from the reserved attributes list, the following tables list the reserved attributes used for Asset and Tag Classifications:
Table 1. Asset Classification Reserved Attributes
Field NameDisplay NameTypeDefault Value
familyTypeFamily TypeStringnull
equipmentTypeEquipment TypeStringnull
makeMakeStringnull
modelModelStringnull
seriesSeriesStringnull
serialNumberSerial NumberStringnull
maintenanceCriticalityRiskScoreMaintenance Criticality Risk ScoreIntegernull
faultModeFault ModeStringnull
Table 2. Tag Classification Reserved Attributes
Field NameDisplay NameTypeDefault Value
uomUnit of MeasureUnitOfMeasurenull
dataTypeData TypeStringString
resolutionData ResolutionStringnull
shiLowThresholdSensor Health Index Low ThresholdDouble0.0
shiHighThresholdSensor Health Index High ThresholdDouble1.00
shiFlatLineNumberSensor Health Index Flat Line NumberInteger720
shiFlatLineEpsilonSensor Health Index Flat Line EpsilonDouble0.00000001
badObservationPersistentBad Observation Persistent / Penalty WindowInteger2880
falseAlarmProbabilityFalse Alarm ProbabilityDouble0.001
missedAlarmProbabilityMissed Alarm ProbabilityDouble0.001
sampleFailureMagnitudesMeanSAMPLE FAILURE MAGNITUDES MEANInteger10
sampleFailureMagnitudesVarianceSample Failure Magnitudes VarianceInteger40
nullHypothesisVarianceNull Hypothesis VarianceDouble0.0025
nanTestWeightNaN Test WeightDouble1
outlierTestWeightOutlier Test WeightDouble1
flatTestWeightFlat Test WeightDouble1
categoryCategoryStringnull
highestThresholdValueHighest Threshold ValueDoublenull
lowestThresholdValueLowest Threshold ValueDoublenull
maxOperatingValueMax Operating ValueDoublenull
minOperatingValueMin Operating ValueDoublenull
aliasesAliasesStringnull

Procedure

  • To enter or modify a single value for a reserved attribute:
    1. In the Applications menu, navigate to HEALTH > Assets > Classifications.
    2. Find and select an Asset Classification or Tag Classification in the Classification results table.
      Tip: You must use the fieldName to search.
    3. In the Reserved Attributes section, hover over a reserved attribute value, and select the Value box to enter a value. The value must match the data type for the attribute. A hint may appear if you enter a value incorrectly.
      Alternatively, you can hover over a reserved attribute value and select , then enter a value in the Attribute Value Definition box.
      Note: You cannot change the datatype of the attribute.
    4. Select Save.
      The entered value is saved and appears in the Value column for the selected reserved attribute.
  • To add and enter or modify multiple values for a reserved attribute:
    1. In the Reserved Attributes section, hover over a reserved attribute value, and select .
    2. Enter a value in the Attribute Value Definition box. The value must match the data type for the attribute. A hint may appear if you enter a value incorrectly.
    3. Select .
    4. Enter an additional value in the new Attribute Value Definition box.
    5. Continue selecting and entering values as needed.
    6. Select Save.
      The entered values are saved and populate the drop-down list box in the Value column for the selected reserved attribute.

Remove Values from Reserved Attributes for a Classification

You can remove values from a reserved attribute for an asset or tag classification.

About This Task

Reserved attributes only appear for asset or tag classifications. You can remove an existing value for a reserved attribute. You can remove multiple existing values for a reserved attribute that contains . Reserved attributes have predefined formatting that cannot be modified. You cannot add or delete a reserved attribute.

Procedure

  • To remove an existing value for a reserved attribute:
    1. In the Applications menu, navigate to HEALTH > Assets > Classifications.
    2. Find and select an Asset Classification or Tag Classification in the Classification results table.
      Tip: You must use the fieldName to search.
    3. In the Reserved Attributes section, hover over a reserved attribute value, and select the Value box to delete a value.
      Alternatively, you can hover over a reserved attribute value and select , then select and delete a value in the Attribute Value Definition box.
    4. Select Save.
      The null value is saved and appears as blank in the Value column for the selected reserved attribute.
  • To remove multiple existing values for a reserved attribute:
    1. In the Reserved Attributes section, hover over a reserved attribute value, and select .
    2. Select the X next to an existing Attribute Value Definition box to delete it. Select and delete the last value from the Attribute Value Definition box if needed.
    3. Select Save.
      The values are removed from the drop-down list box in the Value column for the selected reserved attribute.