Jump to main content
×
Learn more about what Proficy Historian can do for you. Click here for more information on Historian solutions and features.
Get ready for Proficy 2025! Click here to read about our Proficy 2025 offerings.
Delete the Buffer Files of a Collector
About this task
When you delete buffer files, the collector is stopped,
and after the buffer files are deleted, it is restarted.
Procedure
-
Access Configuration Hub.
-
In the NAVIGATION section, under the Configuration Hub
plugin for Historian, select Collectors.
A list of collectors appears.
Tip: You can filter the
collectors by the system name.

-
Right-click the collector instance whose buffer files you want to delete (or
select
), and then
select Clear Buffer.
A message appears, asking you to confirm that you want to clear the
buffer files.
-
Select Clear.
The Clear Buffer: <collector name> window appears.
-
If the collector is running in the command-line mode with a specific user
account, enter values in the USERNAME and
PASSWORD fields.
-
Select Clear.
The buffer files of the collector are deleted.