Jump to main content
×
Learn more about what Proficy Historian can do for you. Click here for more information on Historian solutions and features.
Get ready for Proficy 2025! Click here to read about our Proficy 2025 offerings.
Restore Alarms Using Configuration Hub
About this task Restoring alarms to a running system makes them available
for query and analysis. You can restore alarms that have been backed up or deleted
previously.
Procedure
Access Configuration Hub
In the NAVIGATION section, under the Configuration Hub for
Historian, select Alarms .
The Alarms section appears.
Select , and then select Restore
Alarms .
The Restore Alarms window appears.
In the PROVIDE FILE NAME field, provide the backup file
in the .zip format that you want to restore.
Note: Remember to include .zip at the end of the file
name.
Select Restore .
The alarm data is restored.