Overview of the Simulation Collector

The Simulation collector generates random numbers and string patterns for demonstration purposes. You can configure the number of tags that you want to generate.

Features:
  • The collector generates random scaled values between 0 and 32,767. It uses the high and low engineering units fields of each tag to scale the 0 to 32,767 pre-set values into appropriate engineering units.
  • The collector also provides five-string simulation tags that generate random alphanumeric data.
  • In addition to generating random values, the collector can generate sequential values for some tags. For a list of such tags, refer to Tags with Sequential Values.
  • You can import browse for tags and their attributes.
  • The supported timestamp resolution is 1ms.
  • Floating point, integer, and string data are supported. Binary data is not supported.
  • You can create Python Expression tags.
  • Only polled data collection is supported with a minimum poll interval of 100ms.
Note:
You can create more simulation string tags by manually adding string tags with the following naming convention to the collector: CollectorName.Simulation.StringXXXX
Supported Tag Attributes:
  • Tagname
  • Data Type
  • Hi Engineering Units
  • Lo Engineering Units
  • Hi Scale
  • Lo Scale