Create an RCA using an RCA Template

Steps

  1. Access the RCA Overview page.

    Hint: You can also access the RCA Overview page for a particular Asset Hierarchy Level.

  2. Select the Template tab.

    A list of available templates appears.

    The Template section

  3. Select the row that contains the RCA Template that you want to use to create new RCA, and then select .

    The Template Analysis dialog box appears, asking you to confirm that you want to create a new Root Cause analysis based on the selected RCA Template.

  4. Select Yes.

    The Analysis Summary workspace appears, displaying a datasheet. All the fields on the datasheet are populated from the template except the Analysis Summary field.

    The blank datasheet of an RCA created using a Template

  5. In the Analysis Name box, enter a unique name for the analysis. This is a required field.
  6. As needed, modify the values in the remaining fields, and then select .

    The new Root Cause analysis is created and saved. The list of available analyses on the Templates section is updated.

Results

When you copy an Analysis Template to create a new Root Cause analysis, any of the following items that exist in the original RCA Template will be copied to the new Root Cause analysis:

Copyright © 1993-2016 Meridium, Inc. All rights reserved.