Delete an RCA or an RCA Template

When you delete an RCA or RCA Template, the record is deleted along with all the records that are linked to the Root Cause Analysis except for the:

Steps

  1. Access the RCA Overview page.

    Hint: You can also access the RCA Overview page for a particular Asset Hierarchy Level.

  2. Select one of the following tabs:

    A list of available analyses appears based on the tab that you selected.

    The list of RCAs

  3. Select the row that contains the Root Cause Analysis that you want to delete.
  4. In the upper-right corner of the section, select .

    The Delete Analysis dialog box appears, asking you to confirm that you want to delete the selected analysis.

  5. Select Yes.

    The selected Root Cause Analysis is deleted.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.