Asset Strategy Management Upgrade

Upgrade or Update ASM to V5.2.0.0.0

The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.

Upgrade from Upgrade to Procedure
V5.1.xV5.2.0.0.0
V5.0.xV5.2.0.0.0
V4.6.2 or a later V4.6.x releaseV5.2.0.0.0
  1. Upgrade from any version V5.0.1.0.0 through V5.0.6.0.0
  2. Upgrade from any version V4.6.2.0.0 through V4.6.10.0.0
V4.6.1.x or earlierV5.2.0.0.0
  1. Upgrade from any version V4.6.1.x or earlier to V4.6.2.0.0 or a later V4.6.x release
  2. Upgrade from any version V5.0.1.0.0 through V5.0.6.0.0
  3. Upgrade from any version V4.6.2.0.0 through V4.6.10.0.0
Note: For more information on upgrading to APM V4.6.2.0.0 or a later V4.6.x release, refer to the Upgrade documentation for the corresponding version.

Upgrade from any version V5.1.0.0.0 through V5.1.3.1.0

Action field mappings for Inspection, Calibration, and Proof Test Tasks have been converted from business rules to Policies, as a result any rules-based customization of these mappings will need to be manually implemented using the new mapping Policies via the Action Mapping workspace within the ASM Admin page.

The following baseline queries in the Public\Meridium\Modules\Asset Strategy Management\Management\Queries have been modified and upgraded:
  • Asset Strategy Action Revisions
  • All System Strategy Actions
These queries will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline queries, then you will need to manually update the queries to incorporate the changes.
A Many to Many relationship has been added between the following families:
  • Action and Action Revision
  • Action and Health Indicator
These relationships will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline relationships, then you will need to manually update the queries to incorporate the changes.

Upgrade from any version V5.0.1.0.0 through V5.0.6.0.0

Action field mappings for Inspection, Calibration, and Proof Test Tasks have been converted from business rules to Policies, as a result any rules-based customization of these mappings will need to be manually implemented using the new mapping Policies via the Action Mapping workspace within the ASM Admin page.

The following baseline queries in the Public\Meridium\Modules\Asset Strategy Management\Management\Queries have been modified and upgraded:
  • Asset Strategy Action Revisions
  • All System Strategy Actions
These queries will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline queries, then you will need to manually update the queries to incorporate the changes.
A Many to Many relationship has been added between the following families:
  • Action and Action Revision
  • Action and Health Indicator
These relationships will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline relationships, then you will need to manually update the queries to incorporate the changes.

Upgrade from any version V4.6.2.0.0 through V4.6.10.0.0

This module will be upgraded to V5.2.0.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.