Failure Modes and Effects Analysis Upgrade

Upgrade or Update FMEA to V5.2.0.0.0

The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.

Upgrade from Upgrade to Procedure
V5.1.xV5.2.0.0.0
V5.0.xV5.2.0.0.0
V4.6.2 or a later V4.6.x releaseV5.2.0.0.0
  1. Upgrade from any version V4.6.2.0.0 through V4.6.10.0.0
  2. Upgrade from any version V5.0.1.0.0 through V5.0.6.0.0
V4.6.1.x or earlierV5.2.0.0.0
  1. Upgrade from any version V4.6.1.x or earlier to V4.6.2.0.0 or a later V4.6.x release
  2. Upgrade from any version V4.6.2.0.0 through V4.6.10.0.0
  3. Upgrade from any version V5.0.1.0.0 through V5.0.6.0.0
Note: For more information on upgrading to APM V4.6.2.0.0 or a later V4.6.x release, refer to the Upgrade documentation for the corresponding version.

Upgrade from any version V5.1.0.0.0 through V5.1.3.1.0

The following baseline queries in the Public\Meridium\Modules\FMEA have been modified and upgraded:
  • FMEA Failure Effects and Recommended Actions
  • FMEA Recommended Actions by Type
These queries will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline queries, then you will need to manually update the queries to incorporate the changes.

Upgrade from any version V5.0.1.0.0 through V5.0.6.0.0

The following baseline queries in the Public\Meridium\Modules\FMEA have been modified and upgraded:
  • FMEA Failure Effects and Recommended Actions
  • FMEA Recommended Actions by Type
These queries will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline queries, then you will need to manually update the queries to incorporate the changes.

Upgrade from any version V4.6.2.0.0 through V4.6.10.0.0

The following baseline queries in the Public\Meridium\Modules\FMEA have been modified and upgraded:
  • FMEA Failure Effects and Recommended Actions
  • FMEA Recommended Actions by Type
These queries will be updated automatically when you upgrade the components in the basic APM system architecture. No additional steps are required. If you have modified baseline queries, then you will need to manually update the queries to incorporate the changes.