Button (Classic)
Buttons are used to start any action. By default, the text Submit appears on a button. It indicates that it is used to submit information that an application user provides using other widgets. To use the new version, refer to Button.
Buttons can perform a variety of actions, and can even perform multiple actions. Each specific action has its own choices. For example, if the action of selecting a button is to go to a specific page, that page can be selected after the action is selected in the same grey box.
In addition, you can arrange actions in a sequence. For example, if the selecting a button will both hide a component and submit data entered by a user, the action can first hide the component, and then submit the data, or vice versa.
Button Properties
Field Name | Description |
---|---|
Submit | Sends information to an entity. |
Go to page | Redirects to a different page in the application (for example, from the home page to a different page in the navigation). |
Go to previous page | Redirects to one page back in history based on the entries created
for the current application session. In the absence of previous session entries, the button does not redirect to any page. |
Go to next page | Redirects to one page forward in history based on the entries
created for the current application session. In the absence of forward (next) session entries, the button does not redirect to any page. |
URL | Redirects a user to a URL outside the application. |
Set global value | If selected, the data here will be available globally. Global data means that an entity changed in one part of the application will change across the application. |
Show Component | Displays a hidden component. |
Hide Component | Hides a component. |
Toggle Show/Hide | Some widgets are marked as shown or hidden and the Toggle Show/Hide action will switch between hidden and shown views of a component. |
Visual
- Primary
- Secondary
- Positive
- Negative
- Link
Possible Uses
Buttons can be used for a variety of purposes. In general, buttons are used in conjunction with other widgets. For example, if a user makes a series of selections with drop-down list boxes, check boxes, and radio buttons, they can then select a Submit button that will record the user’s choices in an entity. Buttons can also be used to refresh a page, send a user to another page, set a global value, or show/hide content depending on how the button is configured.
- Add a button widget in the page designer.
- Add a container below the button widget, and provide an ID for the container.
- In the container, add several input widgets, and set the display condition of the container to Hidden.
- In the Button Properties section of the button, set the action of Show Component, and specify the container ID.
- Save the application, and preview it.
In the application, if you select the button, the container appears.