Text Area (Classic)

The text area widget allows a user to provide large amount of text using an application. This widget contains a scroll bar. To use the new version, refer to Text Area.

Text Area Properties

To use a text area widget, in addition to the default settings, the following settings are available.
Field Name Description
Source The source of data based on which queries have been added in the Page Data section. You can also enter the data source manually or use a formula.
Required Identifies if an input must be sent to the query.
Submit on Charge If selected, changing the value of the input submits the query to which this input is assigned.

Possible Uses

A standard text box can handle large amounts of text, but it may not be user-friendly because not all of the text can be seen or edited at once. If a user wants to submit a comment, for example, a text area allows them to write several sentences and view the text as a paragraph (for example, license agreement or privacy policy, which usually contains a large amount of text).