Text Area
Use this plug-in to create a text area to include large text.
To use the old version, refer to Text Area (Classic).
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Text Area Properties
Field Name | Description |
---|---|
Target > Output Value | See Set Up Data Binding for Widgets |
Source > Input Value | See Set Up Data Binding for Widgets |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of Decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. |
Height (px, %, etc) | Enter the size of the text area in pixels. |
Hidden | Select this check box if you want to hide the widget.
To show the hidden widget in Operations Hub new
layout, go to Page Visuals
and under Action column,
select ![]() |