Check Box

To use the old version, refer to Check Box (Classic).

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets

Check Box Properties

Field Name Description
Target > Output Value Selecting the check box in the end app sends value to the target. See Set Up Data Binding for Widgets
Source > Input Value Provides input for the check box from a data source. See Set Up Data Binding for Widgets
Source > Label (unchecked) This is the label that appears when the check box is not selected.
Source > Label (checked) This is the label that appears when the check box is selected.
Label Styling Formats the label: Font Family, Font Size, and Font Color formats the label text.
Check State Colors Select colors that appear in the background of the check box.
  • Unchecked Background Color: This color appears when the check box is not selected.
  • Checked Background Color: This color appears when the check box is selected.
Hidden Select this check box if you want to hide the widget. To show the hidden widget in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden widget. See Page Visuals Tab.