LIKE Operator with Wildcards

The LIKE operator is used with wildcard characters to compare a string to a pattern, and return matched values from the database.

You can use these wildcards with LIKE to build your pattern:

  • % The percent symbol stands for zero or more characters in a sequence.
  • _ The underscore symbol stands for only one character. This single character can also be a number or any punctuation character.
Note:
If using the MS Access database, use these wildcards instead of % (percent) and _ (underscore):
  • * Asterisk to represent zero or more characters in a sequence.
  • ? Question mark to represent a single character.

The LIKE pattern is case insensitive, and is set in single quotes. Employ % and _ with any other character/s (denoted by XY in the table) to search through your database. The wild cards can also be used in combination.

Pattern Description
LIKE '%X' Returns values that end with X. These values can have zero or more characters before X.
LIKE '%XY' Returns values that end with XY.
LIKE 'X%' Returns values that start with X. These values can have zero or more characters after X.
LIKE '%X%' Returns values that contain X. These values can have the X character in any position (start, end, second, fourth, etc.)
NOT LIKE '%X%' Returns values that do not contain X.
LIKE 'X%Y' Returns values that start with X and end with Y. These values can have zero or more characters between X and Y.
LIKE 'X_' Returns values that start with X and has one character after X.
LIKE 'X___' Returns values that start with X and has three characters (3 underscores) after X.
LIKE 'X__Y' Returns values that start with X and end with Y, and has two characters (2 underscores) between X and Y.
LIKE 'X__%' Returns values that start with X and has two characters (2 underscores) after X, followed by zero or more characters.
LIKE '%_X_%' Returns values that contain X if matches with these rules:
  • X cannot be in the first or last position.
  • Implies atleast 3 characters including X.
  • Can have zero or more characters before and after the 3 characters.