Globals
Globals are variables with a global scope, and are available to use with all the widgets/plug-ins in Operations Hub.
Globals are applied outside of a query. A global enables multiple widgets/plug-ins to
access the same data. You can also declare globals as:
- Page Global: Indicated with P, this global variable is applicable only to the page. By default, any global you create is set as a page global. This means it is only accessible and changeable on the specific page where it was created.
- App Global: Indicated with A, this global variable is
applicable to all the pages in an application. If you need a variable to be
available across multiple pages, then you must change a page global to an app
global.
In case you need to change an app global back to a page global, you must make this change on the original page where the global was created. This ensures that the scope of the global is correctly narrowed down to the specific page. A warning message appears when attempting to change an app global. The warning will direct you to the original page where the global was created.
Note:
If multiple widgets/plug-ins use the same Source Input (query), then the
target global must be unique. The global is applicable to the last assigned
widget/plug-in.
- For example, consider
abc
,xyz
, and123
as globals. You can assign each of these global variables as input only once on a page. - If you first assign
abc
to a radio button as input, and assigned it later to a slider as input, thenabc
is applicable as input for the slider plug-in.
To modify an added global, select to switch between Page Global and App Global.


You can create the following types of globals in Operation Hub:
- System Globals: These are global variables used to store computer system related information such as system-wide settings, or configuration parameters.
- Output Globals: These are global variables meant to be used as an output. The output global can be used to store the result of a query. This output global can be accessed and used without having to run the query again.
- UI Globals: These are global variables that can be used on any part of the user interface (UI). For example, a UI global can contain the current user's name and be used to display the user's name in multiple parts of the UI.
- Custom Globals: These are global variables defined by the user. For example, a custom global can be used to store a configuration setting, or a shared resource.
- URL Parameters: These are global variables that store the parameters added towards the end of a URL, which pass additional information to a web server. A URL parameter global can be used to pass information that is required by multiple web pages. For example, the current user's session ID or a referral code.