Copy an Entity (Classic)

This topic describes how to copy an entity.

Before you begin

Log in to Operations Hub.

About this task

You can also create a new entity without copying an existing entity.

Procedure

  1. In the main navigation menu, select ENTITIES.
    The ENTITIES workspace appears.

  2. Select the entity that you want to copy.
  3. Select Edit Entity Structure.
  4. As needed, add or remove fields.
    Tip:
    You can also modify the type of a field by selecting a value in the TYPE column.
  5. Select Save As New.
    The Please enter new name window appears, displaying the name of the entity that you have selected, appended with a system-generated value.
  6. As needed, modify the name of the entity, and then select OK.
    The selected entity is copied.