Delete an Entity (Classic)

This topic describes how to delete an entity in the Operations Hub classic version.

Before you begin

Log in to Operations Hub.

About this task

You cannot delete a baseline entity, an entity that is locked, or an entity that is used in a query.
Note:
In order to unlock an entity, you need to select the entity, click Edit Entity Structure, and then click the lock icon (in the upper right corner) of the Edit Entity Structure page. After you complete that task, you can go to entity list page to delete it.

Procedure

  1. In the main navigation menu, select ENTITIES.
    The ENTITIES workspace appears.

  2. In the rows containing the entities that you want to delete, select the check boxes.
  3. In the workspace heading, select , and then select Delete entities.
    A message appears, asking you to confirm that you want to delete the entities.
    Tip:
    Alternatively, in the row containing each entity that you want to delete, select , and then select Delete entity.
  4. Select OK.
    The entities are deleted.