Copy a Page

Steps to copy a page in the latest version of Operations Hub.

Before you begin

Log in to Configuration Hub.

About this task

For steps to copy pages in the Operations Hub classic version, refer to Copy a Page (Classic).

Procedure

  1. On the navigation panel, select Operations Hub > Applications.


    The existing list of applications and their pages appear.
  2. Right-click the page you want to copy, and select Duplicate Page.


    You can also duplicate multiple pages at a time. To do so:
    1. Select , and then select Page Actions.


      A selection check box appears next to each page.
    2. Select the check box for page you want to duplicate.
      Note:
      To select/clear a check box, you must first select the page in the list.
    3. Right-click and select Duplicate Pages.
    A confirmation message appears.
  3. Select Ok to confirm the duplicate action.
    The Select an Application screen appears.
  4. From the drop down list, select the application to which you want to copy this page.
    You can copy page/s from one application to another, and also within the same application.
  5. Optional: You can modify New Page Name.
    The New Page Name field is already populated with a unique system-generated value.
  6. Select Ok.


Copy a Page (Classic)

Steps to copy a page in the Operations Hub classic version.

Before you begin

Log in to Operations Hub.

About this task

For steps to copy pages in the latest version of Operations Hub, refer to Copy a Page.

Procedure

  1. In the main navigation menu, select APPS.
    The APPS workspace appears.

  2. In the Name column, select the application that contains the page that you want to copy.
    The PAGES workspace appears.

  3. Select the check box for the page you want to copy and choose one of these options.
    OptionDescription
    Copy a single page Select in the row, then select Duplicate page.
    Copy multiple pages Select in the header, then select Duplicate Pages.
    A confirmation message appears.
  4. Select OK to proceed to duplicate the page/s.
    Select an Application screen appears.
  5. From the drop down, select the application to copy this page.
    You can copy page/s from one application to another, and also within the same application.
  6. Provide a name for the page.
    OptionDescription
    Copy a single page Enter a name for the duplicate page. The name must contain at least one uppercase or lowercase letter.
    Copy multiple pages By default, unique names are assigned to each duplicate page.
  7. Copying page/s from one application to another requests for handling globals.
    • Duplicate Globals: Creates page globals with a different name. Recommended when globals have the same name but are of different types.
    • Attempt to reuse Globals: Reuses the page globals. Does not create new globals with the same or duplicate name.
  8. Select OK.
    The pages, along with the UI components, queries, and global variables used in them, are copied.