Create a Page

Steps to create a page in the latest version of Operations Hub.

Before you begin

Log in to Configuration Hub.

About this task

When you create an application in the latest version of Operations Hub, a deafult first page is also created. The following steps show you how to create additional pages for an application.

For steps to create pages in the Operations Hub classic version, refer to Create a Page (Classic).

Procedure

  1. On the navigation panel, select Operations Hub > Applications.


    The existing list of applications appear.
  2. For the application you want to create a new page:
    • Select > Add New Page
    • Right-click and select Add New Page.


    The Create Page screen appears.
  3. Enter the following field values:
    Field Name Description
    PAGE NAME Name of your application page.

    The name must contain at least one uppercase or lowercase letter.

    DESCRIPTION Brief description of your page.
    LAYOUT Based on your page design requirements, select a layout.
  4. Select Add.


    The page is created and a blank page designer screen appears. Refer to Panels Layout.
  5. From the components panel Visuals tab, drag-and-drop or double-click the plug-ins you want to add to the page designer area, and configure their properties.
  6. From the components panel Data tab, bind data to the plug-ins.
  7. On the toolbar, select Save.

Create a Page (Classic)

Steps to create a page in the Operations Hub classic version.

Before you begin

Log in to Operations Hub.

About this task

For steps to create pages in the latest version of Operations Hub, refer to Create a Page.

Procedure

  1. In the main navigation menu, select APPS.
    The APPS workspace appears, displaying a list of applications created in the site.

  2. In the Name column, select the application in which you want to create a page.
    The PAGES workspace appears.

  3. Select Add new page.
    The Create Page window appears.

  4. Provide values as described in the following table.
    Field Name Description
    Page name Enter a name for the page. The name must contain at least one uppercase or lowercase letter.
    Page description Enter a description for the page.
    Include in app navigation Select this check box if you want this page to be included in the application navigation. By default, this check box is selected.
  5. Select Create.
    The page is created, and the page designer appears.

    The container and the left/right panels on the page designer are flexible to use.
    • Drag the left/right sides of the container to resize for a wider view.
    • Select and to show or hide left/right panels.
  6. As needed, add components to the page.
  7. As needed, add queries to the page. Set options for the query, including query submission options.

    Several queries require the multi-select parameter to be selected on the App Page, otherwise no output data will be displayed.

    The following Historian REST queries require the multi-select input to be enabled on the EndApp page for output data to be displayed:
    • Get > Raw Data
    • Get > Calculated Data
    • Get > Sampled Data
    • Post > Calculated Data
    • Post > Interpolated Data
  8. Bind the inputs and outputs of widgets to page data, such as manually entered values, queries, formulas, and globals.
  9. Select Save App.
    The changes made to the page are saved.
    Note:
    At any point in time, if you attempt to navigate away from the page, a confirmation message appears to confirm whether you want to stay on the page, and finish your work.