Export a Model (Classic)

Steps for Operations Hub classic version.

Before you begin

Log in to Operations Hub.

About this task

Model configuration is exported and saved to a CSV format for later use.

Procedure

  1. Go to ADMIN > Import/Export.
    The Model Import/Export screen appears.
  2. You have the option to export the complete model, or only a part of it.
    To export the complete model, do the following:
    1. Enter a file name for the model you want to export.


    2. Select Export.
      The model data is exported to a .csv file.
    To partially export the model, do the following:
    1. Select the check box for Export Partial Model.
    2. From the dropdown list, select a node to serve as a starting point for the export.
      The dropdown list contains all the objects within a hierarchy. For more information on navigation hierarchy, refer to Set Up Runtime Navigation (Classic).
    3. Select Navigation or Containment.
      In Navigation export file, the objects are arranged according to their navigation hierarchy.
      In Containment export file, the objects are arranged according to their parent-child relationship.
    4. Enter a file name for the model you want to export.


    5. Select Export.
      The model data is exported to a .csv file.
    Note:
    The data source connectivity information in the model is not preserved during export. As an alternative, export the application.
  3. Retrieve the model file from the Windows Downloads folder.