Configure Kiosk Mode
This topic provides steps to configure Operations Hub for kiosk mode.
Before you begin
Procedure
-
Open the following URL on the device browser:
https://ophub-host/app/autologin
And the following form will be displayed:The Set up this client device for Kiosk mode form appears. -
Enter the details as described below:
Field Description Username User name used for pre-authenticated application loading. Password Password for the user account. Application URL URL of the Operations Hub end-application. Test Credentials Select this button to test the pre-authentication in a new browser tab based on the credentials and application URL entered in the form. This test does not use persisted data (any data already saved to the device).
-
Select Save to save the entered login credentials and
application URL to the client device.
To remove the saved data (persisted credentials) on the device, select Clear. This is useful when you want to clear sensitive data to re-purpose or decommission the client device.Note:Clearing the browser cache also clears the kiosk pre-authorization credentials. If kiosk mode is required and you cleared the browser cache, then re-run the setup for kiosk mode.The URL that appears at the bottom of the configuration form is the actual URL to start the Kiosk mode. You can copy the link to use at runtime. You may use this for testing, and note that the persisted data will be tested, unlike the Test Credentials button.
-
Once the device is properly configured, access the following URL using the browser
on the client device:
https://ophub-host/app/autologin?kiosk
This is the same URL that appears at the bottom of the configuration form.