Modify Registry for TLS 1.2

This topic describes how to modify the registry setting on the Operations Hub server to allow for TLS 1.2.

About this task

The following steps serve as a workaround to troubleshoot these issues:

Procedure

  1. Access the following registry paths and modify the DWORD value name SchUseStrongCrypto with the value data as 1.
    • HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\.NETFramework\v4.0.30319
    • HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Microsoft\.NETFramework\v4.0.30319
  2. If the registry value does not exist, then create a new one with the same value name and value data.
    Note:
    For more information, refer to Microsoft suggested actions.