Set up Batch
This topic describes how to set up Proficy Batch REST API.
Before you begin
- Proficy Batch Execution ISO file
- Batch REST API zip file
- Latest Batch SIM file
Note:
You also require a GE Digital Batch License Key with Batch Integration Services
and Electronic Signatures for the Batch computer.
About this task
Procedure
- Log in to the machine where Operations Hub is installed.
-
Run the ISO file to install the Proficy Batch Execution application with default
settings.
To create a Windows user account for the batch executive, provide the User name and Password details.
After installation,Batch Execution
folder is created on your desktop. - Install the latest Batch SIM.
- Restart your machine.
-
Unzip the
BatchRestAPI
file and place the folder in your C drive.
-
From the command prompt, run the installation for
BatchRestAPI
service.
-
Access the Readme file in the unzipped
BatchRestAPI
folder and follow the instructions for installation.For example,Country Name US State or Province Name Massachusetts Locality Name Boston Organization Name GE Organization Unit Name Digital Common Name Enter your server name Email Address ophubuser@gmail.com Enter Export Password Enter a password. You must modify the
batch_config_rest_service.json
file to reflect this password. -
From the unzipped
BatchRestAPI
folder, openbatch_config_rest_service.json
in a text editor. For example, Notepad.Refer to the BatchRestAPIReadme.txt
for more details. -
Verify and update these parameters:
serverCertificatePassword
Enter the export password. basicAuthWindowsGroupValidation
If true
, then the Windows user (used for basic auth and for bearer token security) should be a member of the Windows user group indicated by the propertybasicAuthWindowsGroup
. This is initially set toPROFICY_BATCH_REST_USERS
. You must create this Windows group on the Batch REST Service computer, and add the corresponding Windows users to this group.Set this to
false
if you do not want to use Windows Group validation.basicAuthWindowsGroup
PROFICY_BATCH_REST_USERS
uaaServers
Enter the URL for Operations Hub Proficy Authentication (UAA). Note:Only one UAA server is supported.
- Ensure that the Operations Hub user is also a domain user or a local Windows user on the batch computer system. Refer to Configuring Windows User Accounts on the Batch REST Service Computer.
-
From the
Batch Execution
folder, launchServer Manager
.The BatchServerManager application screen appears. -
Select
.
Important:- Use the Windows Services to start/restart the
BatchRestService
after you start/restart the Batch Server. - If
BatchRestService
fails to start, stop the VBIS service and try again. If it still fails, check for error messages in thelogs\batch_rest_api.log
file. Look for a syntax error in thebatch_config_rest_service.json
file, which may be responsible for theBatchRestService
to not start. - Remember to restart
BatchRestService
if you make changes to thebatch_config_rest_service.json
file. - You can also start your Batch Client if you want to compare the data screens with the batch widgets.
- After the Batch REST Service starts, it can take a minute before it is available to receive REST calls.
- Use the Windows Services to start/restart the
-
From the
Batch Execution
folder:Note:You can perform this step right after installing the ISO file as well.