Troubleshooting Install Issues
Issue: SSL Certificate not updated
An SSL certificate allows you to access Enterprise Edition Web Client using HTTPS. You can either use a self-signed certificate or get a trusted certificate from a Certificate Authority (CA).
You must use utility.sh located at plantapps-enterprise-webclient-<buildno> folder to apply the certificate. If the certificate is not updated correctly, navigate to <Install file path>/plantapps-enterprise-webclient<buildno>/log/ansible.log to see the log files.
Refer to the below table, for issues related to certificates and corresponding resolutions.
Issue | Reason | Resolution |
---|---|---|
If utility fails | Not a valid path |
Note:
If the Certificate is signed by Enterprise CA, then it should contain all
certificate levels: the Root CA, the Intermediate Enterprise Certificate, and the
Server Certificate. |
Expired certificate | Replace the expired certificate with the new certificate. If UAA certificate is expired, replace the public keys of the remote services. If Web Client certificate is expired, refer to: Replace the SSL Certificate of Enterprise Edition Web Client. |
|
Certificate not reflecting in the Web Client | Self-signed certificate is not updated, or the certificate is expired | This issue is fixed in PA2022. The PApamymachinesservice
stack was not removed which prevented the certificates to be configured properly.
You must remove the PApamymachinesservice stack by running
the
command:
For more information, refer to: Replace the Public Keys of Remote Services. |
Un-authorization error | Proficy server certificate failed | Access the access control service and check for the PKIX errors, if
found:
|
HAProxy error | Web Client application not accessible | To verify the logs, run the command:
and check for the
HAProxy error: [ALERT] (8) : config : parsing
[/usr/local/etc/haproxy/haproxy.cfg:34] : 'bind *:5059': No Private Key found in
'/usr/local/etc/haproxy/haserver.pem.key'To troubleshoot the HAProxy error:
|
Issue: Unable to access the Enterprise Edition Web Client
Plant Applications Enterprise Edition Web Client is installed only on a Linux machine. After successful installation, application is not accessible and Haproxy service logs display the following errors:
[NOTICE] (6) : haproxy version is 2.5.1-86b093a
[NOTICE] (6) : path to executable is /usr/local/sbin/haproxy
[ALERT] (6) : [haproxy.main()] Cannot raise FD limit to 8251, limit is 1024
Follow the below steps to troubleshoot the issue:
- Modify the following parameter at:
/etc/sysconfig/docker
OPTIONS="--default-ulimit nofile=1024:4096"
Replace with
OPTIONS="--default-ulimit nofile=10000:15000"
- Restart the docker.
Issue: Plant Applications Server Fails to Install
The Plant Applications Server 2023 did not successfully install because of the following error: Failed to create MESCore views and trigegrs. (Proficy.MESCore.DataModelLoader.exe exited with error code.

Please check for the ADO connection failed message in the <Drive>:\Program Files (x86)\Proficy\Proficy Server\Database\SetupLogFiles\VerifyDB.log.
The message indicates that the password has a special character(s).
Follow the below steps to troubleshoot the issue:
- Change the password for the SQL user configured in 'Configure Database' Utility if it contains any special characters.
- Update the password in the 'Configuration Database' Utility and select Save.
- Saving the Database Configuration details takes some time. Once the configuration details are saved, run the Plant Applications Server installation again.