Configuration Parameters in the ERP Export Service
As a system administrator, you can configure the following parameters in the ERP Export service and the Property Definition application in Plant Applications Web Client.
If you have installed Enterprise Plant Applications Web Client, these parameters are available in the following file:
<installation
path>/PlantApplicationsDocker/plantapps-web-docker/erpexportservice.yml.
After you change the values of parameters, run the following Docker commands, and
restart the ERP Export
service:
docker-compose -f erpexportservice.yml config > PAErpExportService.yml
docker stack deploy -c PAErpExportService.yml PAErpExportService
Tip:
If you want to the change the value of a parameter only for the
running instance of the service, you can use a third-party tool such as
Portainer.
If you have installed Standard Plant Applications Web Client, these parameters are available in the following file: C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\erp-export-service\prod\<version>\erp-export-service-prod.properties. After you change the values of parameters, restart the ERP Export service.
Parameter | Description |
---|---|
erp.outbound.messages.messageType | The format of the message. Provide one of the following
values:
|