What's New in Plant Applications 2022

This topic provides a list of product changes released in Plant Applications 2022.

Plant Applications Installation Changes

Table 1. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F57623 Supports silent mode installation and upgrade for Plant Applications Server.
F57624

Supports the following:

  • Silent mode installation and upgrade for Standard Web Client
  • Automatic posting of Web Client applications into Operations Hub.

Application-Wide Changes

Table 2. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
US481336 All the applications in Plant Applications now have more visible column separators in the column headers of the grids, with which you can resize a grid's column as needed.
F61710 Displays the custom user display message that is mapped as an output parameter for a Pre or Post call. The display message is returned to the UI upon success and fail of the pre or post calls if the value is not null, blank or space(s).
F61709 Added Pre and Post custom calls support capability for BOM item consumption and BOM item selection. You can set up the custom calls for both the BOM item consumption and the BOM item selection actions in the Configuration application’s Custom Calls tab.
Note:
Pre call is not applicable for BOM item selection; only Post call is applicable. However, both the Pre and the Post calls are applicable for BOM item consumption.
To facilitate this enhancement, in the Configuration application’s Custom Calls tab, in the Actions section, BOM Item Consumption and BOM Item Selection are added. This feature applicable to Configuration, Process Orders, Unit Operations, and Work Queue.
F58982 Enhances search capabilities for manual BOM consumption. When you search for a serial/lot during manual BOM consumption, a list of serials/lots that match the search criteria appears, along with the number of the search results and the quantity of the selected serial/lot to consume. If you know the exact serial/lot, you can consume the exact serial/lot. If you do not know the exact serial/lot, and/or if you want to consume multiple serials/lots, you can consume multiple serial/lot.

To facilitate this enhancement, a new search button ( ) is added in the BOM section of the Work Queue, Unit Operations, and in the BOM Details section of the Process Order applications. The BOM Details tab is added in the Process Order application.

This feature is applicable to Process Orders, Unit Operations, and Work Queue.

F59924 Provides the ability to determine if a certain variable requires eSignature.
F60758

Updated the Master/Slave Unit terminology to Parent/Child for the following user interfaces:

  • Administrator
  • Excel Add-in
  • Web Report Server, Reports, and Dialogs
  • Thick Client components
  • Web Client components
  • Documentation

This is applicable to Plant Applications Thick Client, Thin Client, and Add-ins.

F33750/US520021

In Route Editor, you can now make required operations with the same sequence number (priority) as mutually exclusive.

So, in Work Queue, if any action is performed on an operation that is a part of the mutually exclusive set, by default, the other operations are mutually excluded. Whereas, in Unit Operations, you will not be able to view the operations that are excluded from the mutually exclusive set.

To facilitate this enhancement, the following changes are made:

  • In Work Queue, a new column called Excluded QTY is added to the grid in the Queue section.
  • In Unit Operations, the operations that are excluded from the mutually exclusive set are not displayed.

In Non Conformance, the following changes are made:

  • When a non conformance is disposed as CTP to an operation in a mutually exclusive set, all the operations in that mutually exclusive set will go on hold by default.
  • In the list of operations to be reworked, the excluded operations from the mutually exclusive set will not appear.

This feature is applicable to Work Queue, Unit Operations, and Non Conformance.

F58015

The filter selection is now persisted for a user for the following applications:

  • Work Queue
  • Work Order Manager
  • Unit Operations
  • Activities
  • Process Order

Reset Grid to Default option is introduced in the settings ( ) that enables you to reset the grid of an application to default.

00993005

Enhanced performance for the following:

  • Loading of receivers having more than 500 Serial Numbers or 500 samples within a lot.
  • Navigating between Inspection Criteria and Inspection Results screen.

Activities

Table 3. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F61196

Adds filtering and enhanced search capability to the Autolog form. The Autolog form provides the following enhancements:

  • New Value column
  • Ability to filter records based on "no Value" or "-"
  • Ability to filter variable values that are out of specification
US488394 The Customs tab functionality is added to the Activities application. The custom tab enables you to create, modify, delete, and add input parameters.

Web Client

Table 4. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F46621

Extends Comment Service V2 to the following process applications:

  • Activities
  • Downtime
  • Process Order
  • Waste Management

There is no change in security level.

The Comment Service V2 converts the old V1 window into a RichText window that allows users to:

  • Apply style sheet to the text.
  • Attach images and videos.
F58015

Supports Persist Record Grouping functionality for the following applications across login sessions in 10% and 90% screens

  • Work Order Manager
  • Unit Operations
  • Work Queue
  • Activities
  • Process Order

Using this functionality, users can now:

  • Save the searched text that includes grid filters and goto search.
  • Persist filters and groupings across login sessions.
  • Use the Funnel icon to reset the filters.
    Note:
    When a filter is applied, the Funnel icon is enabled and clickable.

Plant Applications Security

Table 5. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F59233 Adds a Plant Applications user name in the Proficy Authentication database when the LDAP user log into the Plant Applications Client using Operations Hub.
F57239 All user passwords stored in the Plant Apps database are encrypted.

Receiving Inspection

Table 6. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F49702 Activates workflow for destructive testing and checks the completion of receiver.
F61312 Allows to update values from Common Criteria for all samples.
F49857

Provides the following enhancements to the Receiving Inspection interface:

  • Ability to scan the Receiver number using a Camera.
  • Ability to display scanned records in a different row for a Receiver number.
US511221

Now you can set Variable Alias name and display it instead of Variable name in the Receiving Inspection application. The variable alias name helps you to understand the type of variable easily.

To facilitate this enhancement, the following changes are made:

  • In Plant Applications Administrator’s variable sheet, to set a variable alias, a new column called Variable Alias is added.
  • To control the display of the Variable Alias field instead of the Variable Name field, in the app properties YML file, a property called DisplayVariableAlias is added. You can set the property as True to display the Variable Alias field.
F49700

In Receiving Inspection, we can now compose comments at the following levels:

  • Receiving Inspection level
  • Lot level
  • Test (quality variable) level

To facilitate this enhancement, to compose comments at lot level and test (quality variable) level, a new button () is added in the Inspection Criteria section. To compose comments at Receiving Inspection level, a new button () is added in the Inspection Criteria section.

US516355

In Non Conformance, we can now dispose a non-conformance defect that was created from Receiving Inspection.

To facilitate this enhancement, in Non Conformance, the following dispositions are added:

  • SRAP
  • REWORK
  • MRB
  • RTV
  • DIT
  • ACCEPT
  • RISK RELEASE
US520027/F63169

In Receiving Inspection, if you optionally use an unapproved supplier status for a receiver, the receiver goes on hold.

To facilitate this enhancement, the following change is made:

The on hold ( ) status indicator is added.

US520028/F63169

In Receiving Inspection, you can now view the test history details like under which unit and line the test was created, the current value, when it was entered, who performed the test, and who verified the test.

To facilitate this enhancement, the following change is made:

In the Inspection Criteria section, in the column that lists all the samples (either for a lot or a lot’s variable), a new button () is added. To view the test history, you can select the button and then select Show Test History.

US520029/F63169

In Configuration, you can now add custom and standard tabs for Receiving Inspection.

To facilitate this enhancement,

  • In Standard Tab, Receiving Inspection is included in the list of Applications.
  • In the Custom Tab, Receiving Inspection is included in Tab Association.

In Receiving Inspection, you can now add prefix and suffix to the samples that you create for serialized samples materials.

To facilitate this enhancement, the following changes are made:

  • In the Edit Traceability’s Add subsection, PREFIX and SUFFIX fields are added. You can enter any alphanumerical value with any special characters. For example, AV-2022.
  • The validation of duplicate serial numbers happens along with the concatenation of the string that you entered.

This feature is applicable to Configuration.

US520031/F63169

In Receiving Inspection, while submitting inspection results, you can now select multiple serials/lots at once and update the status.

Note:
  • For multiple selection of serials/ lots, you can change the status only in the following sequence:
    • Open to MRB/NCR or Accept
    • MRB/NCR to Open
  • You can only accept the serials/ lots that have all conforming tests.
  • You can mark the serials/ lots that are not inspected (quality variables are not filled) as MRB/NCR directly.

To facilitate this enhancement, the following changes are made in the Inspection Results section:

  • Checkboxes are added in all the serials/lots rows.
  • To select multiple serials/lots at once, a checkbox is added on the header row of the grid.
  • A dropdown to select the status is added.

Configuration

Table 7. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F60996 Supports pre-release validation on route release before approval workflow.

Web Reports (Classic)

Table 8. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F59254 Supports transferring files without using File Transfer Protocol (FTP) when the Web Report Engine is installed on the same machine as the web server.

Process Order

Table 9. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
US512471 We now have the ACTUAL PRODUCED QUANTITY column in the Process Order application’s Open and Closed pages, with which, you can view the actual produced quantities for a closed or an open process order, in their respective pages.

Work Order

Table 10. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F61139

Supports the following features:

  • Allows SN/Lot to repeat for different materials on the same line
  • ERP: Display Serial number/ Lot wise status changes to material lot when sending back receiver
  • Allows to regenerate samples
F39751 Enhances the performance for work order execution.
F59730

Via the Work Order Manager web application users with permission can add serials/lots to not started work orders.

Via Work Order Manager, Unit Operations or Work Queue Web applications, users with permission can add serials to started work orders that produce serialized parts.

F59731 When creating work orders, or adding lots to a work order, via the web applications, the lot identifiers can be auto filled with numerical or alphabetical increments based on a prefix.
F60781 Support for configuring routes to require manual completion of work orders when all the lots are completed. User with secure permissions can manually complete the work order via Work Order Manager application.

Work Order Manager

Table 11. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F57304 Via Work Order Manager Web application, users with permission can cancel not started lots from ready or in progress work orders.

Route Editor

Table 12. Enhancements and New Features
Tracking ID Description
F33750/US520020

In Route Editor, you can now make required operations with the same sequence number (priority) as mutually exclusive. So, if you perform one operation, then the other operation need not be performed.

To facilitate this enhancement, the following changes are made:

  • To make the operations with same sequence number mutually exclusive, in the Edit Route page, a toggle control is added for all the operations in the grid. You can switch the toggle to make the operation as mutually exclusive to another operation.
  • A new column called Mutual Exclusion is added to the grids in the following sections:
    • Overview
    • Attributes
F50349

Labor planning allows you to specify the amount of time to be spent by labor (people, machines) on operations (segment, planned unit). These times are specified when you create or edit a route.

Labor plans can be exported or uploaded to external schedulers (including ERPs) to inform execution planning and scheduling decisions. Labor plans are not used by execution; however, labor records created during execution might be used to compare execution against plan along multiple dimensions, including operator, line, product, and so on.

F58518 The Pending Approvals tab is added to the Route Editor application. This enables you to attach an approval workflow before releasing the route. Once all the approvals are completed, the route will be moved to released status. The route is moved back to the draft status if it is rejected at any level during the approval process.
F62578 It is possible to have mutually exclusive operations in routes. The Work Queue and Operator applications will allow the operator to clock on to one of the operations in the mutually exclusive set and will mark all the other operations in the set as "excluded". This will also be visible in the work order manager and the History tabs of the work order.

Work Queue

Table 13. Enhancements and New Features
Tracking ID Description
F58952

In Work Queue, we can now change the default value of 50 serial/lots for multiple selection during the following operations:

  • Clock on
  • Clock off
  • Record

To facilitate this enhancement, to change the default value, a new property LotsToExecute is added in the following path:

  • If you have installed Enterprise Plant Applications Web Client, this parameter is available in the following file:<installation_path>/PlantApplicationsDocker/plantapps-web-docker/mnt/configfiles/workqueue-app/prod/<version>/workqueue-app-prod.properties
  • If you have installed Standard Plant Applications Web Client, this parameter is available in the following file: C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\workqueue-app\prod\<version>\workqueue-app-prod.properties

After you change the value of the parameter, restart the Work Queue application.

Alarms

Table 14. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F39714

A new feature, Alarms, has been added to the Plant Applications Web Client. This feature provides a detailed list of alarms that users can view and monitor. The list includes alarms that are:

  • Open
  • Completed
  • Acknowledged

Alarms are configured for the following:

  • To document alarm conditions in addition to reasons and actions
  • For real-time and historical analysis
  • To expose exception-based operating procedures
  • To provide quality control and dispositioning

Waste

Table 15. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
US513315 When creating a waste record, you can now specify the unit for which you want the waste record to be created. To facilitate this enhancement, a UNIT box is available when you create a waste record. When you select a unit, only the events associated with the selected unit are listed in the Event box.

BOM Editor

Table 16. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F56963 Ability to add BOM Family and Master BOM using Web BOM Interface.
US511220 We now have a validation to restrict the precision of decimal places to less than 11. While you enter a BOM formulation, BOM formulation item, and their upper and lower tolerance values, you can enter up to 10 decimal places only. To facilitate this enhancement, in the BOM Editor application, if you add a value greater than 10 decimal places in these fields, a notification message appears, stating that you have exceeded 10 decimal places.
F56963 Ability to add BOM Family and Master BOM using Web BOM Interface.
US464303 We now have a validation to restrict the precision of decimal places to less than 11. While you enter a BOM formulation, BOM formulation item, and their upper and lower tolerance values, you can enter up to 10 decimal places only. To facilitate this enhancement, in the BOM Editor application, if you add a value greater than 10 decimal places in these fields, a notification message appears, stating that you have exceeded 10 decimal places.

Genealogy

Table 17. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F57519 We now have a new BOM section in Genealogy, with which you can view all the associated BOM items and their roll-up (cumulative) consumption history.
F57515 Via the Genealogy Web application, a serial/lot(s) consumed BOM items and used in lots are presented in a graphical view that supports forward and backward crawling to the generalogical view.

My Machines

Table 18. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F57354

Provides a new feature, Inclusive to the My Machines application. Using this feature, users can now:

  • Build their profiles to a narrow view before adding it to the users profile.
  • Clear the existing profiles.

Non Conformance

Table 19. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F60891 Supports additional fields such as Defect ID, Defect Summary, and so on to the NC Main page and the NC Disposition.
F61520/US499216

In Receiving Inspection, we can mark both serialized and non-serialized items that belong to a lot as periodic inspection and generate samples.

If the periodic inspection is delayed, but the material itself is acceptable to use, you can raise a non-conformance and release the other items that belong to the lot at risk.

To facilitate this enhancement, the following are added:

  • In the Receiving Inspection’s Edit Traceability section, a new Periodic Inspection column with a check box is added in the grid. You can select this check box to select an item for periodic inspection, and then generate samples.
  • In Receiving Inspection, the periodic inspection status indicator ( ) is added.
  • In Non Conformance, Risk Release is added as a disposition type. You can release the other items of the lot from which you generated the periodic inspection sample, at risk (either to use or perform inspection).

Route Management

Table 20. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F57169

Ability to display material custom properties and values in the Route Editor application for the following:

  • For a route that creates a specific material.
  • For a configured BOM item.
F46777

Allows users to edit properties on a route by a selecting a value from the drop-down list. Using the drop-down list, users can:

  • Search and filter selected properties
  • Add 100+ values to a single property
  • Select a datatype when building the custom list via the custom table
F62737 The route web service supports exporting a route definition into JSON and XML formats. It is recommended to leverage this web service when retrieving the route definition of a released route vs. leveraging the mes.erp.outbound.message route release content. It is a known issue the definition is this message is incomplete.
F56193

Allows users to define RichText custom property and edit the default value for a property of data type RichText. The RichText functionality supports the following:

  • Property Definition Application
  • Route Editor Application
  • Work Order Web User Interface
  • ERP Import
  • ERP Outbound

Approval Cockpit

Table 21. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F53696

Ability to archive or delete Workflows from the Approval cockpit. An archived Workflow:

  • Can be created only by the user who has created the Workflow or assigned to it.
  • Cannot be triggered.
  • Can activate the Workflow back from the archive.

Downtime

Table 22. Enhancements and New Features
Tracking ID Description
US526044

Ability to export and download the downtime events data in the following format:

  • CSV
  • Excel

ERP Integration

Table 23. Enhancements and New FeaturesThe following enhancements and new features have been added.
Tracking ID Description
F61176

ERP import supports editing some properties for started/in progress process orders:

  • Planned start and end dates
  • Planned quantity
  • Status

When updates are made, ERP outbound messages are generated upon successful processing of the inbound change request.

F59917

ERP import supports editing some properties for started/in progress work orders:

  • Planned start and end dates
  • Planned quantity
  • Priority

When updates are made, ERP outbound messages are generated upon successful processing of the inbound change request.

F59745 Added mes.erp.outbound.messages.operationCancelledEvent that is triggered when a serial/lot is cancelled for an operation. Lots are cancelled from operations when they are split or scrapped.
F51303

Displays an ERP Outbound message that includes custom properties for the following:

  • Work Order
  • Operation Complete

The Work order create, delete, update, status change and complete outbound messages include these custom properties:

  • Work order properties
  • Material lot properties of the produced material
  • Material lot properties of any raw material of a BOM item
  • BOM item properties for route BOM item
F57419 Displays ERP Outbound message that includes all available dimensions of a produced material. For example, for a produced material of certain thickness (y) and height (z), the ERP Outbound message includes dimensional data such as DIM_Y and DIM_Z.
F59744 Added mes.erp.outbound.messages.operationSkippedEvent that is triggered when a serial/lot is skipped for an operation. Lots can be skipped manually by an operator or implicity by the operation when they start the next operation.
F57368 Added support for subscription to events for inbound ERP scheduler requests. When a request is sent to ERP scheduler to import, a kafka message is generated when the import request has been processed indicating whether that import request was successful or not. ERP scheduler web service also supports query by scheduler jobs status and messages.
F62050 Adds the property "DispositionUpdated" to the Material Status Change message at a sublot level. Using this property, the Material Status Change can now indicate if there is an NC raised against it.
F61177 ERP import supports changing the status of a not started work order to cancelled.
F56454 The Materia Lot Import message now allows the external system such as an ERP to define the Inventory Line and Inventory Unit on which the material lot can be created. If this is not specified in the material lot import document, it will pick the Inventory Line and Inventory Unit as defined in the Property Definition application.