ReadBetweenSQL
ReadBetweenSQL can accept the following arguments in the string:
Argument | Data Type | Description |
---|---|---|
?TagId | varchar(1000) | If called from the Administrator, contains the search string entered by the user. If called from a service, contains the tag configured in the variable sheet or model. |
?StartTime | datetime | Start time from which to query from. |
?EndTime | datetime | Endtime from which to query up to. |
?NumValues | int | The number of values to be returned. |
?IncludeExactStart | int | An option that specifies whether to return a data point that is equal to the timestamp (for example, data points >= ?TimeStamp), as opposed to data that is only greater than the timestamp. |
?IncludeExactEnd | in | An option that specifies whether to return a data point that is equal to the timestamp (for example, data points >= ?TimeStamp), as opposed to data that is only greater than the timestamp. |
?HonorRejects | int | - |
ReadBetweenSQL must return data in the following format:
Order | Field | Data Type | Description |
---|---|---|---|
1 | Timestamp | datetime | Timestamp of the data point. |
2 | Value | Value of the data point. | |
3 | Status | varchar(10) | Quality of the data point and has to be one of two values, ‘Good’ or ‘Bad’. |
An example stored procedure for the ReadBeforeSQL is as follows:
CREATE PROCEDURE dbo.spServer_HistorianReadBetween
@TagId varchar(1000),
@StartTime datetime,
@EndTime datetime,
@NumValues int,
@IncludeExact int,
@HonorRejects int
AS
SET ROWCOUNT @NumValues
SELECT TimeStamp,
Value,
‘Good’
FROM MyHistorianTable
WHERE Tag_Id = @TagId
AND ( TimeStamp < @Timestamp
OR ( TimeStamp = @Timestamp
AND @IncludeExact = 1))
ORDER BY TimeStamp ASC