Alerts Management

About Alert Actions

In the inbox and details page of an alert, you can perform various tasks.

Claim or Release an Alert

Before You Begin

Claiming an alert allows you to take ownership of an alert, select its disposition, and create a case for the alert.

Note:
  • You cannot claim or release a claim for an alert that belongs to another user.
  • When you release an alert, you automatically lose subscription to that alert.

About This Task

Claiming an alert in the New state changes its status to Assigned. If an alert is Assigned, you cannot claim the alert until it has been released by the current owner.

Procedure

  • To claim an alert:
    1. In the module navigation menu, select Alerts.
    2. Select , and then select the alert filter set.
      The alerts inbox for the selected filter set appears.
    3. Select an alert in the alerts queue.
      The selected alert appears.
    4. Select Claim Alert.
    The alert status changes to Assigned with you designated as the owner, and the alert moves to the My Alerts filter queue.
    Note: You can select the My Alerts filter to view claimed alerts.
  • To release a claim:
    1. Select , and then select Release Claim.
      The alert returns to the Unclaimed filter queue.

Results

Releasing an alert causes it to revert to a New status.

Assign an Alert

Before You Begin

An analyst can assign an alert that belongs to another user.

You must have Manage Alerts permissions to assign an alert to another user.

Procedure

  1. In the module navigation menu, select Alerts.
  2. Select , and then select the alert filter set that contains the alert that you want to assign.
    A pane that contains a list of alerts appears.
  3. Select the alert.
    A section that contains the details of the alert appears.
  4. Select , and then select Assign Alert.
    The Assign Alert window appears.
  5. Select the text box, and then in the Search box that appears, enter at least one character of the user name.
    A list of user names populates with the matching characters.
  6. From the list, select the user to whom you want to assign the alert.
  7. Select Assign.

Results

The name of the user appears as the owner in the ALERT INFORMATION section, and the user is now subscribed to this alert. In addition, visibility for this alert is set to Limited.
Note: When you assign an alert to a user who does not have access to the alert, and does not have Manage Alerts permission, a message appears indicating that the alert was not assigned.

Assign an Alert Disposition

Before You Begin

After claiming an alert, you can assign a disposition to indicate its validity. Dispositions are retained when you release, process, or reclaim an alert.
Note: You cannot assign a disposition for an alert that belongs to another user.

About This Task

In the Alerts grid view, the default value for Disposition is None. The Disposition column is required in the grid. The Disposition column can be sorted as well.

Procedure

  1. In the module navigation menu, select Alerts.
  2. Select , and then select My Alerts to display the claimed alerts.
    A pane that contains a list of claimed alerts appears.
  3. Select the alert to which you want to assign a disposition.
    A section that contains the details of the alert appears.
  4. In the Disposition drop-down list box, select one of the following options:
    Disposition CategoryDisposition Code
    Potential IssuePotential Issue
    Potential Issue - Diagnosis
    Potential Issue - Recommended Actions
    Potential Issue - Post Outage Change
    Potential Issue - Operational
    Sensor ProblemSensor Problem

    (Pre-6.0 was Potential Issue - Sensor Problem)

    ResolutionResolution
    Resolution - Sensor Required
    Resolution - Catch
    Resolution - No Action Taken
    Resolution - Operational Change
    Resolution - Scheduled Maintenance
    Resolution - Unplanned Maintenance
    Resolution - Forced Outage
    Resolution - Model Maintenance Successful
    Resolution - Customer Remediation
    Resolution - Customer Resolved
    Resolution - Other
    Asset MaintenanceAsset Maintenance
    Asset Maintenance - Bad Training Data
    Asset Maintenance - Load Out of Range
    Asset Maintenance - Ambient Out of Range
    Asset Maintenance - Operational Change
    Asset Maintenance - Turn Off Bad Tag
    Asset Maintenance - Threshold Adjustment
    Asset Maintenance - Other Adaptation
    Asset Maintenance - Other Configuration
    Asset Maintenance - Post Outage Change
    MonitoringMonitoring
    Monitoring - Notification to Customer
    Monitoring - Under Customer Review
    Monitoring - Response from Customer
    Monitoring - Customer Action Pending
    Monitoring - Questions for Subject Matter Expert
    Monitoring - Under Subject Matter Expert Review
    Monitoring - Response for Monitoring Analyst
    Monitoring - Request for Maintenance Engineer
    Monitoring - Question for Customer
    Transient
    • Transient
    • Transient - Startup
    • Transient - Load
    • Transient - Shutdown

    Your selection results in the following workflow actions:

    • Selecting False, False - System, or Outage invalidates the alert.
    • Selecting Valid, Sensor Issue, or Reset State Date acknowledges that the alert needs further investigation, and you can begin your analysis.

Mark an Alert as Dismissed

About This Task

You can mark a claimed, Assigned alert as Dismissed to indicate that the alert no longer needs attention.

Procedure

  1. In the module navigation menu, select Alerts.
  2. Select , and then select My Active Alerts to access alerts claimed by you.
    A pane that contains a list of alerts appears.
  3. Select an alert claimed by you.
  4. Select , and then select Dismiss Alert.

    The alert is removed from the My Active Alerts queue.

    Note:

    To find the processed alert, select All Alerts Filter, and then search by Status.

Add or Delete Notes in an Alert

Before You Begin

Notes can help you in clarifying evidence during a diagnosis.

There are two note sections in the details page of an alert, INTERNAL NOTES and NOTES:
  • Internal Notes: The INTERNAL NOTES section appears only if you have either View Internal Notes or Manage Internal Notes permission. If you have the View Internal Notes permission, you can view and read any internal notes, but cannot add or edit the note. The Manage Internal Notes permission allows you to view internal notes and add a note. However, you can delete only your own notes. The INTERNAL NOTES section does not appear in the alerts grid, nor can be exported to a PDF.
  • Notes: The NOTES section is available to all users with View Alert Detail or Manage Alert permission. If you have Manage Alert Detail permissions, you can edit or delete notes. The NOTES section appears in alerts grid as a column, and can be exported to a PDF.

Procedure

  • To add a note:
    1. In the module navigation menu, select Alerts.
    2. Select , and then select the alert filter set that contains the alert for which you want to add a note.
      A pane that contains a list of alerts appears.
    3. Select the alert.
      A section that contains the details of the alert appears.
    4. In the NOTES section of the alert, enter text in the box.
      You can enter up to 5000 characters.
    5. Select Add Note.
      The new note appears in the NOTES section.
  • To delete a note:
    1. Select next to the note.
      The selected note is removed from the NOTES section.

Apply Filters to Alerts

About This Task

You can apply default filter sets to Alerts.

You can use filter sets to narrow queue entries into a manageable set.

Note: The filters applied to the alerts inbox or grid is persistent even if you navigate out of alerts, therefore not requiring you to select the filter attributes again until you log out of the application. This is valid for a given user session.

Procedure

  1. In the module navigation menu, select Alerts.
  2. Select , and then select a filter set, such as My Alerts or Unclaimed.
    The filter is applied to the alerts inbox or alerts grid.

Create a Case from an Alert

To initiate and track the process used to address an issue identified in an alert, you can create a case from the corresponding details page of the alert.

Before You Begin

You must have Alerts permissions and Cases permissions to create a case from an alert.
Note:
  • You can create a case for an alert that belongs to the same tenant.
  • When you create a case from an alert and if the EVIDENCE section of the alert contains an analysis chart, the same analysis chart will be available in the EVIDENCE section of the case.

About This Task

You can create a case from an alert by providing an Asset ID at any level (enterprise, site, segment, or asset).

Procedure

  1. In the module navigation menu, select Alerts.
  2. Select , and then select My Alerts.
    A pane that contains a list of alerts assigned to you appears.
  3. Select the alert for which you want to create a case.
    The details page of the alert appears.
  4. Select Create Case.
    The Create Case window appears.
  5. In the Title box, enter a case name.
  6. In the Symptoms box, enter a description, and then select Save.

Results

A case with the selected name and severity appears in the LINKED CASES section of the alert. The case then becomes available in the Cases module.

If you create multiple cases for a single alert, the Case Number in the Case Information section is incremented by one for each additional case.

Access a Case from an Alert

About This Task

When you create a case from an alert, the case is generated in the Sentinel Web Cases module, and a link to the case appears in the LINKED CASES section in the details section or page of an alert.

Procedure

  1. In the module navigation menu, select Alerts.
  2. Select and then select the alert filter set that contains the alert for which a case is created.
    A pane that contains a list of alerts appears.
  3. Select the alert.
    The details page of the alert appears.
  4. In the LINKED CASES section, select the linked case that you want to view.
    The Limited Visibility Cases appear in the LINKED CASES section only if you have the View Limited Visibility Cases permission. Otherwise, only the General Visibility Cases are displayed in the LINKED CASES section of the alert.

Results

The case details of the selected case open in a new web browser tab.