Set Attribute with Attribute
Description
Set Attribute with Attribute updates an attribute value with another attribute value.
Parameters
This function block has the following parameters:
Parameter | Description |
Destination Region ID | ID of Region where item is located. |
Destination Location | Location of the item in the Region. |
Destination Item Class | Class of the item. |
Destination Attribute ID | ID of Attribute whose value is to be set. |
Source Region ID | ID of Region where item is located. |
Source Location | Location of the item in the Region. |
Source Item Class | Class of the item. |
Source Attribute ID | ID of Attribute whose value is to be used to set the Destination Attribute ID. |
Source Attribute Start Char | Specify the start character if setting a substring of the source Attribute. |
Source Attribute Length | Specify the number of characters to set starting from Source Attribute Start Char. |
Pseudo Code
Read source attribute value
If attribute is found
Read destination attribute
If attribute is found
Update destination attribute value with the source attribute value.
End if
End if
Note: System attributes cannot be modified.