Set Decision Status
Description
Set Decision Status sets the current decision status, which can hold a 16-character string defined by the user.
This is the decision that is currently being selected by the RCO. You cannot change the decision status until a decision has been selected. If no decision has been selected (Many decisions still possible) or all decisions have been eliminated (None still possible) then nothing happens when the block is executed.
Note: The decision status is displayed in the RCO_UI decision history list.
Parameters
This function block has the following parameters:
Parameter | Description |
Value | User defined 20-character string. Value can be typed in or can be set from an RCO Variable. |
Pseudo Code
Not available for this release.
Return Value
None.