Set Attribute with Value
Description
Set Attribute with Value updates an attribute with a value.
Parameters
This function block has the following parameters:
Parameter | Description |
Region ID | ID of Region where item is located. |
Location | Location of the item in the Region. |
Item Class | Class of the item. |
Attribute ID | ID of Attribute whose value is to be set. |
Value | Value or RCO Variable which is written to the specified attribute. |
Note: System attributes cannot be modified.