Highlight Event

Highlight triggers a procedure or calls a script after an object in CimView changes from not highlighted to highlighted.

Field Description
A Action Contains a drop-down list of existing procedures and scripts. Use either of the following.
Procedure    
Script    
B Parameter Can be used if the event invokes a script directly or through a procedure. The default code begins as follows. Sub OnHighlight(highlightReason As Long) Where parameters are:
highlightReason  
C Debounce event Check      
Clear      
Note:
When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.
Note:
When the Highlight event is configured for an object, a CimView user can highlight the object by:
  • Placing the mouse cursor on it.
  • Tabbing to it.
  • Using the arrow keys to select it.