Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmBackupResponseHandler Delegate
Whether this is the final response.
Overall operation status.


AlarmBackupResponseHandler Delegate
A delegate invoked for Alarm/Events Backup Response.
Syntax
Public Delegate Sub AlarmBackupResponseHandler( _
   ByVal final As System.Boolean, _
   ByVal status As Status _
) 

Parameters

final
Whether this is the final response.
status
Overall operation status.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also