Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiFieldValue Class
Members


MultiFieldValue Class
This is the structure of the data written to a tag of type MultiField
Syntax
Public Class MultiFieldValue 
Inheritance Hierarchy

System.Object
   Proficy.Historian.ClientAccess.API.MultiFieldValue

Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also